cancel
Showing results for 
Search instead for 
Did you mean: 

GPIOs configurations in low-power Standby Mode: STM32G0B1RET

Kmax18
Senior II

I am using this MCU on a battery-supplied custom board: STM32G0B1RET.
I am looking for clarification re. the GPIO availability in Standby Mode.
Table 26 in Reference Manual RM0444 (see below) seems to offer one of two (exclusive) possibilities:

  1. Without wakeup capability: wakeup pins are not available, but I/Os can be configured with internal pull-up, pull-down or floating. That would mean a GPIO pin can be assign 0 in Standby Mode.
  2. With wakeup capability: wakeup pins are available, but GPIOs cannot be configured and are floating.

Please confirm. Thank you!

Kmax18_1-1741959775481.png

 

 

 

 

12 REPLIES 12

Try RM0444 chapter 7.3.15, but yes isnt very clean.

@TDK, just for clarification re. the STM32G0B1RET on a battery-supplied custom board:  the datasheet states that the pull-down resistor is weak, Table 55 lists around 40kOhm (see below). Can that cause a problem in Standby mode?
Also, one member states that in Standby Mode only RTC pins can drive low.

Please advise, I look forward to resolving this.

Kmax18_0-1742185622403.png

 

I don't see why that would cause a problem.

Not sure, no board here for me to test. Seems like it should work.

If you feel a post has answered your question, please click "Accept as Solution".