Getting started .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-09-24 1:20 PM
I have the STMf32f469 board , when I try to send a demo to the board it says that I do not have the St link utility ? Shouldnt I have got that with the StmCube install ? Or do I need to download that specifically ?
EDIT> Worked with ST link. Although it is just in one corner of the screen , resolution issue .
Although the demo should be set to 800x480 ? === I can only select the STM32f469I and not the STM32f469. Is my board not supported and is the I version higher resolution ?
Or are the demos made for smaller screens ?
Is there a get started PDf or something somewhere , there is way too much on the STm site and I get confused , can someone point me to a get started thingy ?
Thanks
- Labels:
-
STM32F4 Series