2024-12-03 4:26 AM
Is possible to generate different tone using dac peripheral for triangle wave form generation using PCM sample in stm32 nucleo F410RB controller. Is it possible to generate tone using wav data(pcm array).
1.If possible to generate need to give wav format or not needed?
2. If not which stm32 development board supports dac to generate tones using pcm array's.
Solved! Go to Solution.
2024-12-05 3:57 AM
2024-12-05 4:04 AM - edited 2024-12-05 4:05 AM
I've already shared the link in a previous comment https://community.st.com/t5/stm32-mcus-products/the-audio-player-demonstration/td-p/389084.
The demo is no more available as the board is obsolete one user has shared it on google drive.
2024-12-05 4:27 AM
@AMS12345 wrote:for audio wave file specification, the example code may helps me out.
As noted, that part will not be specific to STM32 - so just do an internet search.