cancel
Showing results for 
Search instead for 
Did you mean: 

G431 will run (somewhat) with debugger, but not on its own.

Tobe
Senior III

I have made a prototype, and it runs as just after upload. But when i just turn on the power, it wont. It does not matter if the st-linkv3 ist connected or not. When i reset it, via the NRST pin, it also wont run.

I already used the HSE and HSI, and checked on a nucleo, that my code is working (it does).

I dont know how i further can investigate this. The level of NRST is clean and the level is good.

1 ACCEPTED SOLUTION

Accepted Solutions
Tobe
Senior III

It works:

I had to set nSWBOOT0 to 0. See picture attached.

Thanks a lot.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

What about Boot pin? connected to VDD or GND?

See for example this thread: https://community.st.com/t5/stm32-mcus-products/stm32h723zgt6-will-not-reboot-after-powering-off/m-p/650457

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

BOOTx pins or settings?

Get a USART working very early in the Reset Handler so you can express signs-of-life. Could perhaps use GPIO/LEDs at as simpler level. Have Hard Fault and Error Handlers output actionable data.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Neither: It is connected to RX of a CAN chip. See attached the waveforms.

pink is Boot0 pin, blue is 3.3V of STM

 

Hello,

Neither: It is connected to RX of a CAN chip. See attached the waveforms.

 

Sorry.. I didn't catch that point!  How did you connect Boot pin? which CAN chip? could you please share schematics?


pink is Boot0 pin, blue is 3.3V of STM


Pink signal is rising. It should be connected to the ground. Why BOOT pin voltage is changing?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
Tobe
Senior III

It works:

I had to set nSWBOOT0 to 0. See picture attached.

Thanks a lot.