cancel
Showing results for 
Search instead for 
Did you mean: 

G431 block diagram missing information

Tobe
Senior III

Hi,

i have two questions here:

A: That line should not be there, so the bar downwards would be the AHB2?

B: This is APB1?

 

5 REPLIES 5
AScha.3
Principal III

you talking about ...?

this: ?

AScha3_0-1701175009927.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Yes, i forgit to include it. I just added it.

 

KDJEM.1
ST Employee

Hi @Tobe ,

Thank you for bringing this issue to our attention.

I will check internally  and I will get back to you with more details as soon as possible.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Take this with you: (it should be right i think)

KDJEM.1
ST Employee

Hi @Tobe ,

I confirm the issue and I reported internally.

Internal ticket number: 167372 (This is an internal tracking number and is not accessible or usable by customers).

Thank you for your contribution in STCommunity 🙂.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.