2022-03-12 12:03 PM
I have NUCLEO-144 H723ZG board.
I created a frequency meter app for the NUCLEO board, but the quality of the frequency measurement a sinusoidal voltage is very poor. I have a generated 720mV RMS, 126.7Hz signal between 0 and +2.5V (max) biased to +1.25V. On scope, the frequency meter connected to the output of the COMP1 shows 126.700x, the 4th digit is 1 or 0. The NUCLEO board measures almost 1Hz less than the frequency meter on scope (I checked it with a real frequency meter and the scope value is right).
My other problem is that the minimum value of the frequency = 125.451, the maximum value = 125.9264Hz, the average = 125.7246 and the standard deviation = 0.0775Hz. I could not measure the frequency as good as a simple scope.
Setup:
I enabled COM1 comparator. I connected the input sine voltage to the positive input (COMP1_INP) and I connected the negative input (COMP1_INN) to the +1.25V reference voltage to which the input signal is biased. With setting the COMP1 speed to “COMP_POWERMODE_HIGHSPEED�? I got terrible output voltage. Both edges of the output are bounced (200-250 spikes) at least 1-3us. Then I set the COMP1 speed to “COMP_POWERMODE_MEDIUMSPEED�? and I got only a couple of spikes. Then I set the COMP1 speed to “COMP_POWERMODE_ULTRALOWPOWER�? and I got no spikes. The hysteresis was always set to “COMP_HYSTERESIS_HIGH�?. Why? Can somebody explain it?
I connected the comparator output with a wire to the Capture Channel 1 input of the 32-bit TIM2. The timer runs on 275MHz (3.636ns) as a simple up counter, with ARR = 0xFFFFFFFF, Prescaler = 0. It is started with HAL_TIM_IC_Start_IT(&htim2, TIM_CHANNEL_1);
When rising edge of comparator detected on the Capture CHN1 input of TIM2 then TIM2 captures the value its 32-bit counter and calls the HAL_TIM_IC_CaptureCallback(). I read the capture 1 register and store the value in last period count if this is the first interrupt. It this is not the first interrupt then I subtract the current count from the last count (I also update the last value register to the current one). This is the period time in counts. I set a flag in the callback function to signal that I measured a new period time count. In the main() loop when this is true then I simply divide the 275MHz TIM2 clock with the period count. This is my measured frequency. Because I don’t have LCD and send it via serial port to the terminal APP of my notebook. The application runs continuously.
Even though this is a simple period time measurement I cannot not answer the following two questions.
Can somebody help. (Sample app for NUCLEO-144 H723ZG board is available if needed)
Thanks for any help, any idea.
Louis
Solved! Go to Solution.
2022-03-18 3:50 AM
Oops, sorry, Jan is right.
Yes, with ST-LINK-V3E you can set the MCO output to one of three possibilities:
I have already crossed out my statement above.
I apologise for forgetting this for a moment.
Regards
/Peter
2022-03-12 12:23 PM
What's the primary clock source?
If it's STLink3's 8MHz output, that is not derived from crystal.
JW
2022-03-12 1:52 PM
Hi waclawek.jan,
Yes, STLINV3 8MHz is the primary clock. The are no other (real) chances. STM does not assemble the 25MHz crystal (X3) and two caps. Without soldering a 25MHz crystal + 2 caps manually into the board, the STLINV3 8MHz is the only chance for the clock source. By the way, the STLINKV3 works from X1 25MHz crystal. Why do you think the 8MHz is not crystal clock? I guess STLINKV3 has a PLL which generates the 8MHz (DIV=25, MUL=8) but I do not know that chip.
Thanks for the idea!
L
2022-03-16 6:28 AM
Dear STMicro,
I really need to know whether the 8MHz primary clock of NUCLEO-144 H723ZG board is derived from crystal or RC oscillator? If this clock is an RC oscillator then it explains the frequency error and uncertainty.
Thanks,
Louis
2022-03-17 8:58 AM
I initialized TIMER 1 to run from 137.5 MHz frequency. I set the prescaler = 0, the period = 100 and set channel 1 to toggle the output. I attached my scope probe to the TIMER 1 channel 1 output pin (PE9, CN10.4) and I measured the frequency . It was anything between 1.371 and 1.373 MHz, instead of 1.375 MHz. It was very unstable.
Still no comment?
March 17, 2022. 18:53:
I modified the prescaler = 5 - 1 and period = 27500. The timer 1 divides with 5 * 27500 = 137500, so I should get 1000Hz. But I get anything between 1006 and 1008 Hz...
???
2022-03-17 12:34 PM
I've told you already that STLink3's 8MHz output is not derived from crystal (which means it's derived from its HSI). And your symptoms confirm it. What's the point of your repeated posts, then?
And no, 'F723 used as STLink3 cannot generate 8MHz from 25MHz.
In CubeProgrammer you probably can switch STLink3's output to a different frequency, derived from the 25MHz crystal. I don't use CubeProgrammer nor STLink3. There are several related threads on this forum, search.
JW
2022-03-17 12:50 PM
OK so you have already been told all this two weeks ago...
JW
2022-03-17 12:51 PM
2022-03-17 1:52 PM
Thank you all of your the answers, ideas.
When I opened this an the two weeks ago topic I was sure the the STM32H723 NUCLEO board runs from a crystal or crystal oscillator. (I did not have the schematic). Then waclawe.jan told me the HSE = 8MHz clock is not derived from crystal. (Then derived from what?) Then I begun to test the timers, and I found that - probably - the HSE clock is generated by an RC oscillator. My symptoms confirmed that. So now, after two weeks, I know the right question. All I want to know is:
How can I run the STM32H723 NUCLEO board from a crystal or a crystal oscillator?
I guess, the only way is to buy the not assembled 25 MHz crystal and 2 x 5.1 pF capacitors and somehow solder those into the board and remove the SB34 bridge.
Thanks and sorry for the duplicated topics.
L
2022-03-18 1:20 AM
Well, as @Community member wrote, the clock for the target STM32H723ZGT6 is fed from the MCO of the ST-LINK-V3E. The ST-LINK-V3E itself is driven by a STM32F723IEK6, in whose clock scheme the MCO outputs can only be fed from four sources and a divider 1:1...1:5 before the output: LSE, HSE, HSI and PLLCLK. Unfortunately, the (non-changeable) MCO frequency chosen for the ST-LINK-V3E is not the HSE, but 8MHz, which cannot be derived from the required PLLCLK, but only from the HSI.
So if you need a crystal stabilised clock on the STM32H723ZGT6, you must indeed could:
[edited: pls see the comments below]
Fortunately, the NUCLEO is only an evaluation or development board and is not used for finished products, so hopefully this is acceptable?
We are very sorry for this inconvenience.
Regards
/Peter