2020-09-17 11:01 AM
I am using a STM32F446re to detect rising edges, calculate the frequency and execute accordingly.
I have two signals that need to be detected. So I use two Timers 3 and 4. My frequency ranges from 3Hz to 300 kHz so I need to use overflow detection.
However When an overflow and a input capture happen close to each other, the overflow is not recognised and the frequency is miscalculated.
How can I check for interrupts within an interrupt routine?
2020-09-17 2:02 PM
uint32_t lastTim3Ccr1, totalTim3Cnt;
void TIM3_IRQHandler(void) {
uint32_t sr, arr, ccr1;
sr = TIM3->SR;
TIM3->SR = ~sr; // clear active flags - we don't intend to change mask ever so don't need to mask here
arr = TIM3->ARR; // this may be a constant, if ARR never changes
if (sr & TIM_SR_CC1IF) { // capture upon edge
ccr1 = TIM3->CCR1;
if (ccr1 < arr / 2) { // may have been yet unhandled overflow before capture
if (sr & TIM_SR_UIF) { // and sure it was
sr &= ~TIM_SR_UIF;
totalTim3Cnt += arr;
}
}
ccr1 += totalTim3Cnt;
ProcessDelta(ccr1 - lastTim3Ccr1);
lastTim3Ccr1 = ccr1;
}
if (sr & TIM_SR_UIF) { // overflow?
totalTim3Cnt += arr; // accumulate total time
}
}
You have to make sure latency is less than arr/2.
JW
2020-09-18 12:13 AM
Thank you JW
This looks good and it is similar on what I was doing with my atmega2560 before.
I am fairly new to STM32 so forgive me my stupid questions.
Am I right that I will insert your code into the stm32f4xx_it.c
void TIM3_IRQHandler(void)
{
/* USER CODE BEGIN TIM3_IRQn 0 */
--->YOUR CODE HERE<----
/* USER CODE END TIM3_IRQn 0 */
HAL_TIM_IRQHandler(&htim3);
/* USER CODE BEGIN TIM3_IRQn 1 */
/* USER CODE END TIM3_IRQn 1 */
}
Also an other stupid question. ProcessDelta is a funktion of the Cube IDE?
I couldn't find anything on it in a quick search.
I will test it tonight and try to educate myself until then on the topic.
Thanks again.
2020-09-19 2:35 AM
> Am I right that I will insert your code into the stm32f4xx_it.c
I don't use Cube. This would be the whole ISR, no need to call HAL_TIM_IRQHandler(&htim3).
> ProcessDelta()
No, I just wanted to say, "insert here whatever code you want to process the time difference".
JW
2020-09-20 6:23 AM
Hello JW
I tried to setup a new project to have a clean start. However the ISR is not triggered.
What am I missing?
I know that the timer is running and the SR register changes when I directly serial print it in the while loop.
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2020 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim3;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM3_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint32_t lastTim3Ccr1, totalTim3Cnt;
volatile uint32_t delta;
char buffer[100];
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_TIM3_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_IC_Start_IT(&htim3, TIM_CHANNEL_1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
// clear active flags - we don't intend to change mask ever so don't need to mask here
HAL_UART_Transmit(&huart2, (uint8_t*)buffer, sprintf(buffer, "%d", delta), 500);
debugPrint(&huart2,";");
HAL_UART_Transmit(&huart2, (uint8_t*)buffer, sprintf(buffer, "%d", __HAL_TIM_GetCounter(&htim3)), 500);
debugPrintln(&huart2,";");
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief TIM3 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM3_Init(void)
{
/* USER CODE BEGIN TIM3_Init 0 */
/* USER CODE END TIM3_Init 0 */
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_IC_InitTypeDef sConfigIC = {0};
/* USER CODE BEGIN TIM3_Init 1 */
/* USER CODE END TIM3_Init 1 */
htim3.Instance = TIM3;
htim3.Init.Prescaler = 400;
htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
htim3.Init.Period = 65535;
htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_IC_Init(&htim3) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
sConfigIC.ICFilter = 0;
if (HAL_TIM_IC_ConfigChannel(&htim3, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM3_Init 2 */
/* USER CODE END TIM3_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @param None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
}
/* USER CODE BEGIN 4 */
void debugPrint(UART_HandleTypeDef *huart, char _out[]){
HAL_UART_Transmit(huart, (uint8_t *) _out, strlen(_out), 10);
}
void debugPrintln(UART_HandleTypeDef *huart, char _out[]){
HAL_UART_Transmit(huart, (uint8_t *) _out, strlen(_out), 10);
char newline[2] = "\r\n";
HAL_UART_Transmit(huart, (uint8_t *) newline, 2, 10);
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
void TIM3_IRQHandler(void)
{
/* USER CODE BEGIN TIM3_IRQn 0 */
uint32_t sr, arr, ccr1;
debugPrintln(&huart2,"Interrupt");
sr = TIM3->SR;
TIM3->SR = ~sr; // clear active flags - we don't intend to change mask ever so don't need to mask here
delta=99;
arr = TIM3->ARR; // this may be a constant, if ARR never changes
// delta= __HAL_TIM_GetCounter(&htim3);
if (sr & TIM_SR_CC1IF) { // capture upon edge
ccr1 = TIM3->CCR1;
if (ccr1 < arr / 2) { // may have been yet unhandled overflow before capture
if (sr & TIM_SR_UIF) { // and sure it was
sr &= ~TIM_SR_UIF;
totalTim3Cnt += arr;
}
}
ccr1 += totalTim3Cnt;
//(ccr1 - lastTim3Ccr1);
lastTim3Ccr1 = ccr1;
}
if (sr & TIM_SR_UIF) { // overflow?
totalTim3Cnt += arr; // accumulate total time
}
/* USER CODE END TIM3_IRQn 0 */
HAL_TIM_IRQHandler(&htim3);
/* USER CODE BEGIN TIM3_IRQn 1 */
/* USER CODE END TIM3_IRQn 1 */
}
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2020-09-20 6:34 AM
Also how do I setup a project without HAL? I think this is messung up my workflow.