2024-09-17 1:00 AM
Hello,
I was wondering if it is possible to use the FreeRTOS Middleware which is used on the STM32H7 and STM32F4 and which can be found at the following links ‘https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Middlewares/Third_Party/FreeRTOS/Source’ and ‘https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Middlewares/Third_Party/FreeRTOS/Source’ in the case of the STM32U5G9VJTxQ. Or if on the other hand, in the case of this chip this Middleware is not valid and it is necessary to proceed in a different way.
Thanks!
Solved! Go to Solution.
2024-09-17 1:19 AM
Hello @EnaitzO ,
Please check these links which contain some FreeRTOS examples for STM32U5 that might be helpful:
2024-09-17 1:19 AM
Hello @EnaitzO ,
Please check these links which contain some FreeRTOS examples for STM32U5 that might be helpful: