cancel
Showing results for 
Search instead for 
Did you mean: 

FMC SRAM not working

ashutoshtekriwal
Associate III

Hello,

We have been using two SRAMs (CY7C1061G30-10BV1XE) & one NAND Flash(MT29F8G08ADAFAH4-AAT) interfaced with STM32L562 micro-controller on same FMC bus. We have initialised FMC and try to access SRAM1 by selecting Chip select: NE1 and Bank 1. It is being observed that there is mismatch between Read and Write Data in Bank 1 (FMC Base address: 0x60000000). Also, we have tried to change the various parameters' values as configurable under FMC Initialisation (like: Byte Lane NBL set-up timing and other SRAM timing parameters), but this all could not help us and data mismatch persists. Also, we suspect that FMC clock frequency which is set as 25MHz in our case. 

Schematic of SRAM, our code and FMC initialisation can be referred below:

(1) FMC_Initialisation:

static void MX_FMC_Init(void)

{

 

/* USER CODE BEGIN FMC_Init 0 */

 

/* USER CODE END FMC_Init 0 */

 

FMC_NORSRAM_TimingTypeDef Timing = {0};

 

/* USER CODE BEGIN FMC_Init 1 */

 

/* USER CODE END FMC_Init 1 */

 

/** Perform the SRAM4 memory initialization sequence

*/

hsram4.Instance = FMC_NORSRAM_DEVICE;

hsram4.Extended = FMC_NORSRAM_EXTENDED_DEVICE;

/* hsram4.Init */

hsram4.Init.NSBank = FMC_NORSRAM_BANK1;

hsram4.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;

hsram4.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;

hsram4.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;

hsram4.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;

hsram4.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;

hsram4.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;

hsram4.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;

hsram4.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;

hsram4.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;

hsram4.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;

hsram4.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;

hsram4.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;

hsram4.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE;

hsram4.Init.NBLSetupTime = 0;

hsram4.Init.PageSize = FMC_PAGE_SIZE_NONE;

hsram4.Init.MaxChipSelectPulse = DISABLE;

/* Timing */

Timing.AddressSetupTime = 2;

Timing.AddressHoldTime = 2;

Timing.DataSetupTime = 2;

Timing.DataHoldTime = 2;

Timing.BusTurnAroundDuration = 2;

Timing.CLKDivision = 16;

Timing.DataLatency = 17;

Timing.AccessMode = FMC_ACCESS_MODE_A;

/* ExtTiming */

 

if (HAL_SRAM_Init(&hsram4, &Timing, NULL) != HAL_OK)

{

Error_Handler( );

}

 

/* USER CODE BEGIN FMC_Init 2 */

 

 

/* USER CODE END FMC_Init 2 */

}

 

(2) FMC Defs (main.h):

#define SRAM_BANK_ADDR ((uint32_t)0x60000000)

#define WRITE_READ_ADDR ((uint32_t)0x0800)

 

(3) Code (main.c):

uint16_t txbuffer=0x1234;

uint16_t rx;

 

if(HAL_SRAM_Write_16b(&hsram4,

(uint32_t *)(SRAM_BANK_ADDR + WRITE_READ_ADDR),

&txbuffer,

sizeof(txbuffer)) != HAL_OK)

{

//return SRAM_ERROR;

printf("ERROR");

}

/* Read back data from the SRAM memory */

if(HAL_SRAM_Read_16b(&hsram4,

(uint32_t *)(SRAM_BANK_ADDR + WRITE_READ_ADDR),

&rx,

sizeof(rx)) != HAL_OK)

{

printf("ERROR");

// return SRAM_ERROR;

}

 

ashutoshtekriwal_0-1716960220488.png

 

2 REPLIES 2
KDJEM.1
ST Employee

Hello @ashutoshtekriwal ,

This issue may be due to a wrong timing configuration, for that I advise you to refer to AN4761 precisely Timing computation section.

I hope this help you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

ashutoshtekriwal
Associate III

We have already gone through AN4761 and timing seems to be correct, we have also tried with increased timings and low clock frequency but nothing works as of now. Kindly suggest some way to debug that timings are fine/correct.