Running HAL_SPI_TransmitReceive causes reset of the STM32L151RBT6A
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-29 7:07 AM
Hi. First time I have posted here. This problem is driving me nuts, so hopefully someone might lead me to a solution. I am under extreme time pressure with this project and need to solve this very quickly. If anyone can help, it would be much appreciated and I'd owe you a beer at least.
I am using STM32cubeIDE ver 1.15.1, generating C code. Code for all I/O functions work fine, except the SPI. In fact, whenever I try to excercise the SPI, the CPU resets. The nRST line on the CPU glitches to 0V and then resets. Nothing Is driving that reset line, other than the S-LINK/V2, so the reset is happening within the STM32L151.
The application is driving on the SPI port two RF chips: the CC1120 and the SX1276. I have checked SPI various lines and there are no shorts and no obvious schematic errors. Both have independent SPI chip selects. Also the RF chips are not producing any RF - the digital signals are all clean.
I was using the SPI nCS line (NSS), with software control from the .ioc file, and thinking there was an issue there for the CC1120, I cut a track and rerouted that signal to PB0. Still same bug.
I have read code examples and even used ChatPGT to generate code. Nothing fixes the issue.
I have attached some screen shots of the schematic. The rail voltages are all 3.0V. Here is a test while(1) loop in main.c, simplified as to not cause confusion. As you can see, I have tried this with having the CC1120 and SX1276 stuck in reset, and only one in reset and none in reset - but no luck.
This is puzzling!
The SPI config is as such:
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
Solved! Go to Solution.
- Labels:
-
SPI
-
STM32CubeMX
-
STM32L1 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-29 7:00 PM
I THINK I FOUND THE CAUSE!
It was that 10K resistor to VDDA. I only put it in there due to a legacy issue on an earlier design by an engineer who died suddenly last year, so I could not ask him why he put that in.
Chat GPT 4 actually say the voltage on the VDDA is important, and if it has the wrong voltage on it (eg: 10K will drop it), it will cause resets from the SPI! ChatGPT is remarkable.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-29 6:07 PM
I found the line of code in stm32I1xx_hal_spi.c that crashed using debug, if that is any help...
{
if ((hspi->Init.Mode == SPI_MODE_SLAVE) || (initial_TxXferCount == 0x01U))
{
*((__IO uint8_t *)&hspi->Instance->DR) = (*hspi->pTxBuffPtr); // CRASHES HERE!
hspi->pTxBuffPtr += sizeof(uint8_t);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-29 7:00 PM
I THINK I FOUND THE CAUSE!
It was that 10K resistor to VDDA. I only put it in there due to a legacy issue on an earlier design by an engineer who died suddenly last year, so I could not ask him why he put that in.
Chat GPT 4 actually say the voltage on the VDDA is important, and if it has the wrong voltage on it (eg: 10K will drop it), it will cause resets from the SPI! ChatGPT is remarkable.