2025-05-10 1:52 PM
I am using a custom PCB with stm32g474 and I am trying to get the CAN peripheral working. I believe I have everything set up correctly (bit rate, RAM etc) but when I call HAL_FDCAN_AddMessageToTxFifoQ(), FIFO is full error is raised after 3 iterations.
Any help is appreciated.
Solved! Go to Solution.
2025-05-13 1:29 AM
I agree 100% with mƎALLEm.
I'm still thinking that You have a problem with the physical Bus.
Do You have the possibility to check the signals on the BUS?
For example with a PC and a Can dongle, or with a oscilloscope.