cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN Clock issue

garry lai
Associate II

fdcan colock error? why?i600.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @garry lai ,

According to your screen shot it seems your MCU is an STM32H7. May be an STM32H743?

If you refer to the RM0433/Table 60. Kernel clock distribution overview:

The table provides the peripheral max clock according to the VOS level you've already set:

SofLit_0-1701438475636.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

3 REPLIES 3
KDJEM.1
ST Employee

Hello @garry lai ,

Could you please give more details:

- Which STM32 devices are you using?

- Which STM32CubeMX version are you using?

Thanks and best regards,

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

AScha.3
Chief III

move your mouse pointer there - a pop up will tell you the max. allowed clock

If you feel a post has answered your question, please click "Accept as Solution".
SofLit
ST Employee

Hello @garry lai ,

According to your screen shot it seems your MCU is an STM32H7. May be an STM32H743?

If you refer to the RM0433/Table 60. Kernel clock distribution overview:

The table provides the peripheral max clock according to the VOS level you've already set:

SofLit_0-1701438475636.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.