2023-12-01 12:40 AM - last edited on 2023-12-01 1:02 AM by KDJEM.1
2023-12-01 5:49 AM - edited 2023-12-01 5:50 AM
Hello @garry lai ,
According to your screen shot it seems your MCU is an STM32H7. May be an STM32H743?
If you refer to the RM0433/Table 60. Kernel clock distribution overview:
The table provides the peripheral max clock according to the VOS level you've already set:
2023-12-01 1:05 AM
Hello @garry lai ,
Could you please give more details:
- Which STM32 devices are you using?
- Which STM32CubeMX version are you using?
Thanks and best regards,
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-01 1:06 AM
move your mouse pointer there - a pop up will tell you the max. allowed clock
2023-12-01 5:49 AM - edited 2023-12-01 5:50 AM
Hello @garry lai ,
According to your screen shot it seems your MCU is an STM32H7. May be an STM32H743?
If you refer to the RM0433/Table 60. Kernel clock distribution overview:
The table provides the peripheral max clock according to the VOS level you've already set: