2021-04-05 6:14 AM
The program to read the Internal temperature and V_battery voltage using ADC in STM#2F042 is as follows:
#include "main.h"
#define I2C_ADDR (0x40<<1);
#define V_Ref 3.3
#define RESOLUTION 255
#define TEMP30_CAL_ADDR ((uint16_t*)((uint32_t*)0x1FFFF7B8))
#define TEMP110_CAL_ADDR ((uint16_t*)((uint32_t*)0x1FFFF7C2))
ADC_HandleTypeDef hadc;
float internal_temp;
uint8_t index1=0;
uint32_t adc_value[2];
float V_bat;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC_Init(void);
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
if(__HAL_ADC_GET_FLAG(hadc,ADC_FLAG_EOC))
{
adc_value[index1]=HAL_ADC_GetValue(hadc);
index1++;
}
if(__HAL_ADC_GET_FLAG(hadc,ADC_FLAG_EOS))
{
internal_temp = adc_value[0];
internal_temp -= (int32_t) *TEMP30_CAL_ADDR;
internal_temp *= (int32_t)(110-30);
internal_temp /= (int32_t)(*TEMP110_CAL_ADDR - *TEMP30_CAL_ADDR);
internal_temp += 30;
V_bat=(float)adc_value[1]*V_Ref/RESOLUTION;
index1=0;
}
}
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_ADC_Init();
MX_TIM2_Init();
HAL_ADC_Start_IT(&hadc);
while (1)
{
}
}
static void MX_ADC_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
hadc.Instance = ADC1;
hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_8B;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
hadc.Init.ContinuousConvMode = ENABLE;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
sConfig.SamplingTime =ADC_SAMPLETIME_1CYCLE_5 ;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_VBAT;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
This is the code I have written (generated from Cubemx.) It will not get the proper value for internal temperature and V_bat (battery voltage).The internal temperature shows 45°C.
Can someone please tell me the error/problem in the code, especially in the callback function?
2021-04-05 6:36 AM
Perhaps output the values you're actually reading, and double check the math on paper.
Start perhaps by casting the pointers properly, via a less convoluted cast
#define TEMP30_CAL_ADDR ((uint16_t*)0x1FFFF7B8)
#define TEMP110_CAL_ADDR ((uint16_t*)0x1FFFF7C2)
and making sure those look to be valid
printf("%u %u\n", *TEMP30_CAL_ADDR, *TEMP110_CAL_ADDR);
As I recall the slope is negative.
2021-04-05 9:48 AM
> The internal temperature shows 45°C.
That's a completely normal internal temperature for smaller packages.