Question
stm32g031j6m6 NRST as output not working
Hello. Using NRST as an output. Initial state 1. After loading, I switch to 0 and the MCU is rebooted :(. I used options PA0, PA1, PA2. If I use PF2, then the output is constant 1. MCU stm32g031j6m6. On the STM32G0316-DISCO board, the same MPU works correctly.
Is there a solution for this MPU?
Designation on the case of the problem MCU 32G031J6 ZK027
Maybe some register is not configured?