F746 using LCD
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-16 6:37 AM
Dear every body,
I are using
LCD TFT 7 inch 800x480/external-link.jspa?url=https%3A%2F%2Fwww.buydisplay.com%2Fdefault%2F7-tft-lcd-touch-screen-display-module-800x480-for-mp4-gps-tablet-pc
in our design with
STM32F746BTG6processor working at 200
MHz frequency.
The data is loaded from SDRAM to LTDC (STM32F7 LCD Controller)
using DMA2D and FMC interface(Flexible Memory Controller – Working at 200/2 MHz).- SDRAM which i'm using:
/external-link.jspa?url=https%3A%2F%2Fwww.micron.com%2Fparts%2Fdram%2Fsdram%2Fmt48lc16m16a2p-6a
MT48LC16M16A2 – 4 Meg x 16 x 4 banks
- IDE: MDK Version 5 - Keil
- Library: HAL.
I have some question to ask you:
How do I enable the frame interrupt ?
How do I disable the SDRAM auto refresh function ?
Please support me.
Thank you!
#f746-using-lcd- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-16 7:10 AM
You should be able to generate a Line interrupt for the LTDC via a position programmed into LIPCR
See:
HAL_LTDC_ProgramLineEvent()
STM32Cube_FW_F7_V1.9.0\Projects\STM32746G-Discovery\Applications\STemWin\STemWin_HelloWorld\STemWin\Target\LCDConf.c
HAL_LTDC_LineEventCallback()
STM32Cube_FW_F7_V1.9.0\Projects\STM32746G-Discovery\Examples\LTDC\LTDC_Display_2Layers\Src\main.c
Not sure of the value of killing the auto-refresh, presumably you feel the display visits rows/columns sufficiently. The SDRAM initialization has a command sent to the chip itself, and a clock count for the controller.
For display ripping consider not modifying the active frame buffer, or getting better optimized routines, the BSP library examples here are rather inefficient.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-25 4:04 AM
Dear you,
I want ask you about step by step LTDC out data to LCD TFT.
What is signalling signal of LTDC to MCU to read data from SDRAM. After that, LTDC out data to LCD TFT.
Example link:
https://m.eet.com/media/1202452/KEOLABS%20figure%jpg
https://github.com/hampussandberg/HexConnect/wiki/Simple-GUI
LTDC can't get data directly from SDRAM. Isn't it?
Thank you!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-25 8:47 AM
Not sure I'm up for generating a step-by-step
The DMA2D is what is classically a Bit-Blit operation, manipulating the frame buffer, see your lower diagram with back-n-forth to SDRAM
https://en.wikipedia.org/wiki/Bit_blit
The LTDC paints the rasters (lines) to the screen, it manages the serialization of the pixel, line and frame data to the display, it reads the frame buffer from SDRAM, and pipes it to the display in the RGB form required, along with any control signalling and clocking.
Up vote any posts that you find helpful, it shows what's working..