2024-09-20 05:17 PM
Hello,
i am working on a board that is redrawn from the H745I-Disco which originally has the FT5336 as touch controller. My Display has the FT5426. On an earlier board that recreated the F746-Disco (which also has the FT5336) i noticed that the FT5426 worked right away. This was not the case on the H745 but was fixed after changing the Device ID. So touches are detected and deliver the proper values for x and y in sampleTouch() but nothing reacts to it. It is like there is no touch functionality at all. Any recommendations?
Thanks in advance!
Martin