cancel
Showing results for 
Search instead for 
Did you mean: 

F4 HAL CRC utility

MM..1
Chief III

Hi , have somebody link to exe or online or linux utility with same result as HAL CRC calculate?

 

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
waclawek.jan
Super User

srecord

JW

Thanks srec line example for bin file ?

https://community.st.com/t5/stm32-mcus-products/stm32f4-crc32-algorithm-headache/m-p/371428

https://community.st.com/t5/stm32-mcus-security/crc-computation/m-p/536190/page/2

// STM32 CRC32 Test App - sourcer32@gmail.com
//  Copyright (C) 2014

#include <windows.h>
#include <stdio.h>
#include <stdlib.h>

//****************************************************************************

DWORD Crc32(DWORD Crc, DWORD Data)
{
  int i;
  Crc = Crc ^ Data;
  for(i=0; i<32; i++)
    if (Crc & 0x80000000)
      Crc = (Crc << 1) ^ 0x04C11DB7; // Polynomial used in STM32
    else
      Crc = (Crc << 1);
  return(Crc);
}

//****************************************************************************

DWORD Crc32Block(DWORD Crc, DWORD Size, DWORD *Buffer) // 32-bit units
{
  while(Size--)
    Crc = Crc32(Crc, *Buffer++);

  return(Crc);
}

//****************************************************************************

DWORD Crc32Fast(DWORD Crc, DWORD Data)
{
  static const DWORD CrcTable[16] = { // Nibble lookup table for 0x04C11DB7 polynomial
    0x00000000,0x04C11DB7,0x09823B6E,0x0D4326D9,0x130476DC,0x17C56B6B,0x1A864DB2,0x1E475005,
    0x2608EDB8,0x22C9F00F,0x2F8AD6D6,0x2B4BCB61,0x350C9B64,0x31CD86D3,0x3C8EA00A,0x384FBDBD };

  Crc = Crc ^ Data; // Apply all 32-bits

  // Process 32-bits, 4 at a time, or 8 rounds
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // Assumes 32-bit reg, masking index to 4-bits
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // 0x04C11DB7 Polynomial used in STM32
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
  Crc = (Crc << 4) ^ CrcTable[Crc >> 28];

  return(Crc);
}

//****************************************************************************

DWORD Crc32FastBlock(DWORD Crc, DWORD Size, DWORD *Buffer) // 32-bit units
{
  while(Size--)
    Crc = Crc32Fast(Crc, *Buffer++);

  return(Crc);
}

//****************************************************************************

void test(void)
{
  BYTE vector[12] = { 0x02,0x07,0x02,0x00,0x18,0x8A,0xD0,0x23,0x25,0x2B,0x09,0x00 }; // ACD7E298
  DWORD Crc;
  int i;

  for(i=0; i<sizeof(vector); i++)
    printf("%02X ",vector[i]);
    putchar('\n');

  Crc = 0xFFFFFFFF; // Initial state

  for(i=0; i<sizeof(vector); i+=4)
  {
    Crc  = Crc32Fast(Crc, *((DWORD *)&vector[i]) ); // 4-bytes at a time
  }

  printf("%08X %08X test",Crc, Crc32FastBlock(0xFFFFFFFF, sizeof(vector)/4, (void *)vector));
}

//****************************************************************************

void TestFile(char *Filename)
{
  FILE *f;
  DWORD Size;
  BYTE *Buffer;

  f = fopen (Filename, "rb");
  if (f)
  {
    fseek(f, 0, SEEK_END);

    Size = ftell (f);

    fseek(f, 0, SEEK_SET);

    if (Size & 3)
      printf("WARNING: File must be multiple of 4 bytes (32-bit) for valid results\n");

    Buffer = malloc(Size);

    fread(Buffer, Size, 1, f);

    fclose(f);

    printf("crc=%08X Slow\n", Crc32Block(0xFFFFFFFF, Size >> 2, (void *)Buffer));
    printf("crc=%08X Fast", Crc32FastBlock(0xFFFFFFFF, Size >> 2, (void *)Buffer));

    free(Buffer);
  }
  else
    printf("ERROR: Unable to open file '%s'\n", Filename);
}

//****************************************************************************

int main(int argc, char **argv)
{
  printf("STM32CRC Test\n  Usage: STM32CRC [<file>]\n");

  if ((Crc32(0xFFFFFFFF, 0x12345678) != 0xDF8A8A2B) ||
      (Crc32Fast(0xFFFFFFFF, 0x12345678) != 0xDF8A8A2B))
  {
    printf("ERROR: Internal Sanity Check Failed\n");
  }

  if (argc > 1)
    TestFile(argv[1]);
  else
    test();

  return(1);
}

//****************************************************************************
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks i compile it on linux after little complication with DWORD. Now it work and result is same thx.

But for other is better have utility ready...

Not exactly rocket sciencery..  but I'll bite.

windows.h contained DWORD

https://github.com/cturvey/RandomNinjaChef/blob/main/stm32crc.c

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

I looked at RandomNinjaChef's menu first, but couldn't find the right flavour of CRC there.

Oh, it's a fresh dish.

JW