F103C6T6A i2c doesn't send start
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-12 11:12 AM
Hello,
I was working with i2c on a f103c6t6a a couple of months ago and it was working.
Now i just update stmcube ide to last version and i cannot get it work again.. (had a problem with gpio settings in past).
What i dont get is:
trying to use HAL_I2C_IsDeviceReady() doesn't seems to work and i always get error 512 a time out waiting SB flag to be set.
So i get stucked there where it keep waiting for SB flag but never comes up.
It sets bit 8 in CR1 and then nothing.
if(HAL_I2C_IsDeviceReady(&hi2c1, (0x40 << 1) , 2, 100) == HAL_OK){
HAL_Delay(10);
}
SET_BIT(hi2c->Instance->CR1, I2C_CR1_START);
/* Wait until SB flag is set */
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_SB, RESET, Timeout, tickstart) != HAL_OK)
{
if (READ_BIT(hi2c->Instance->CR1, I2C_CR1_START) == I2C_CR1_START)
{
hi2c->ErrorCode = HAL_I2C_WRONG_START;
}
return HAL_TIMEOUT;
}
I checked with an other device if the ina219 was working and i got response on its address.
Reading from reference manual start should be
Setting the START bit causes the interface to generate a Start condition and to switch to
Master mode (MSL bit set) when the BUSY bit is cleared.
it doesn't switch to master mode and if busy bit refer to bit 2 in SR2 is clear.
I don't understand what is changed from 2 months ago to make it not working.
Thanks
- Labels:
-
I2C
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-13 7:54 AM
Errata seems to not solve it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-29 3:37 PM
Hi,
It would appear that I have the same problem, (with a STM32F103C8).
I have tried my darndest, and I have other MCUs ESP32, Pico W on the same line that works well, so it shouldn't be any pull-up stuff or anything else hardware related.
I get stuck in exactly the same place with the same error.
@Stequila93​ Have you found a solution?