cancel
Showing results for 
Search instead for 
Did you mean: 

Example of SDMMC on STM32H757 i-EVAL Board

Tteva.1
Associate II

Hi everyone .

I'm looking for a demo code to run the SD card (16gb) with FatFs on the STM32H757 i-EVAL Board.

When I generate it with CubeMx the demonstration doesn't work (I didn't forget to activate the transiver)

Thanks you =)

1 ACCEPTED SOLUTION

Accepted Solutions
4 REPLIES 4
Ons KOOLI
Senior III

Hi Tteva.1,

Can you please share your .ioc file ?

Else, you can refer to the STM32CubeH7 Firmware. You can find examples and applications that can help you.

Best Regards,

Ons.

Tteva.1
Associate II

Hi Ons KOOLI ,

Thanks you for the reply. Yes i can share :)

If you see an error ;)

aasil
Associate II

Hi Tteva.1,

I want generate code with CubeMx for sdmmc1 on STM32H757i- EVAL but it doesn't work ... i used stm32h747.c lib and i also tried to change example of stm32h743- eval (sd_read_write_HS_dma) but it doesn't work...

I'm really confused about ...

do you find any solution for it??

Best Regards,

amir.