I solved it. Thanks, before this I was using 0x480 which didn't work. but now i have another problem when i use external flash touch gfx for widgets make wrong color like blue button-> green button but... (with internal flash everything is fine) do y...
I'm using my custom boad with stm32h743iit6 and I'm trying to put TouchGFX data in an external flash (w25q128). I'm using the quad-spi.
So, I make an external loader and It seems to work properly. if I load the .stdlr file in the STM32CubeProgrammer ...
Hi Tteva.1, I want generate code with CubeMx for sdmmc1 on STM32H757i- EVAL but it doesn't work ... i used stm32h747.c lib and i also tried to change example of stm32h743- eval (sd_read_write_HS_dma) but it doesn't work...I'm really confused about ....