cancel
Showing results for 
Search instead for 
Did you mean: 

Error on compiling of the buck-boost example of AN4449

vguil
Associate

Hello,

I would like to use the example of AN4449 on SW4STM32.

When building, I have 3 errors :

fatal error: opening dependency file Drivers/BSP/STM32F3348-Discovery/stm32f3348_discovery.d: No such file or directory

make: *** [Drivers/BSP/STM32F3348-Discovery/stm32f3348_discovery.o] Error 1

recipe for target 'Drivers/BSP/STM32F3348-Discovery/stm32f3348_discovery.o' failed

How can I solve this issue?

0 REPLIES 0