2022-08-23 04:50 AM
Error in final launch sequence:
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
Why?
2024-06-18 11:07 PM
CAN YOU PLEASE GIVE THE SOLUTION FOR THIS.
I try everything for this but not solved this issue.
2024-07-28 10:38 AM
Did u get the solution
2024-08-22 05:08 AM
Hello, I have the same probleme and I don't find how to solve it on the web
2024-09-02 01:40 AM
Hi @ADębs.1 any news?
2024-09-03 07:03 AM
same problem
2024-09-03 07:20 AM
But, i have resolve my problem (bad config) :
"Debug configuration..." > "Debugger"
- Change : "[X] Connect to remote GDB server" to "[X] Autostart local GDB serveur".
- Chek if "Debug probe" is "ST-LINK (ST-LINK GDB serveur).
- And : "[X] ST-LINK S/N" and press "[Scan]".
2024-09-04 06:20 AM
@S3b i have tried but nothing. my st link is hot when i touch it
2024-09-04 07:08 AM
Make sure both of the st-link jumpers on your board are exist.
2024-10-04 11:40 PM
What fixed the issue for me was removing a misplaced jumper that was causing the board to be stuck in the reset state. Check the user manual of your board for what jumpers are needed for what function, then remove the jumpers that are out of place. You can search "jump" or "JP" to make searching the manual faster.