2022-08-23 4:50 AM
Error in final launch sequence:
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
Why?
2022-08-25 8:00 AM
Hello @Andrzej Dębski ,
Try erasing the flash using STM32Cubeporgrammer, and make sure to activate the gdb server log in the "Debugger" tab of your debug configuration, this may helped you.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2022-08-25 9:29 AM
Is the device local or remote, check settings and expectations.
2022-08-26 6:58 AM
Local device
2022-08-26 7:23 AM
Can you please provide a meaningful title for your request?
Many thanks
2022-08-26 9:08 AM
Perhaps screen shot the debugger settings you have in the tool currently. It will help to understand the "not working"
What board or STM32 is involved here?
How is it connected?
Is the ST-LINK connected directly? And not via a hub or docking station.
Hard you tried better cables?
Does STM32 Cube Programmer work/connect properly?
Understand its very hard to debug this stuff with no information or context.
Explain the situation better and more completely.
2022-11-18 5:25 AM
@Andrzej Dębski Where you able to solve this issue in the end?? Because I am having the same problem.
2023-04-10 4:55 PM - edited 2023-11-20 9:09 AM
[SPA] En nuestro caso la falla se solucionó recargando el proyecto con otro nombre. Cambiamos el cable y el cable no era el problema. El proyecto anteriormente trabajaba sin problemas, pero luego de rearmar el circuito y volver a cargar el codigo en el programa presento la falla. Esa fue la solución en nuestro caso usando la tarjeta STM32F411RE con CubeIDE 1.10.1
2024-02-03 11:29 PM - edited 2024-02-03 11:30 PM
I am having the same problem. CubeIDE 1.14.1
2024-03-01 4:46 AM
I am having the same problem cube ıde and cube ıde programming, won't you help?