2024-10-04 10:42 PM
Hi, ST.
I want to know if the stm32h7(h750vb) series supports sdio? The spec sheet only describes the SDMMC peripheral (memory card etc.), but I want to use SDIO in my project to connect with esp32 to use WIFI (using esp-hosted library). I want to know if there is a way to achieve it?
Thanks!
2024-10-05 12:06 AM
Hello @PickaxeHit and welcome to the ST Community
As you said the STM32H750VB integrate only 2 SDMMC interfaces. But if we go to the paragraph 3.39 of the DS12556, we can fin that the SDMMC support MMC,SD and SDIO card.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.