2023-03-18 4:10 AM
Hello,
i found an error in the Datasheet DS12712 Rev 4 of the STM32G473 Controller.
Can someone clarify please what will be correct:
In Chapter 4.11 - "Alternate functions" it tells, that PA10 has an alternate funktion AF2 for I2C3_SCL
But in Chapter 4.10 - "Pin definition" the I2C3_SCL is not listet for pin PA10 in the Alternate functions column.
So will the I2C3_SCL be available at PA10 or not?
Solved! Go to Solution.
2023-03-21 1:37 AM
Hello @Moritz ,
A new DS revision will be published as soon.
I will get back to you when the issue is fixed.
Thanks,
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-18 4:51 AM
2023-03-21 1:37 AM
Hello @Moritz ,
A new DS revision will be published as soon.
I will get back to you when the issue is fixed.
Thanks,
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.