2014-11-26 07:21 AM
So,
*
Timing Parameters for write and read access if the Extended Mode is not used
Wrong!
Parameter used for read operation.
Check FSMC_NORSRAMInit( *p) from stm32f4xx_fsmc.c it without assert()2014-11-27 08:06 AM
Hi,
Could you please provide more details on the error you are reporting:- What is the used SPL version?- Which parameter?...-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.