2014-11-27 5:38 AM
Hi,
I am currently working with the stm32f030 MCU and I am trying to configure I2C timing and the MCU clock, peripheral clocks.I got this excel sheets from ST (what were they thinking?) where you can configure the I2C and clocks but it wont work on excel 2010, and I cannot find it officially on their homepage no more either. They have this ''Cube'' software which I do not really want to use and that does not really help me generating the configuration files I need, like system_stm32f0xx.c. I cannot find anything that helps me with the I2C timing either in this Cube tool.Anyone have any suggestions? Did I miss something?Regards,Rygelxvi2014-11-27 9:12 AM
Hi,
Do you mean ''The clock configuration tool'' when you speak about the excel sheet? Is it the one that you can download fromhttp://www.st.com/web/en/catalog/tools/PF257924
?If you want to use the SPL, you can refer to the I2C examples in the standard peripheral library (http://www.st.com/web/en/catalog/tools/PF257884
).The Cube also contains some examples.So, you can choose the more suitable solution in your case.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.