Erasing flash sector works, but writing it causes HARD FAULT
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-09 3:49 AM
I am trying to write data in the flash of an STM32F446RE, sector 5.
My linker script is configured so that .user_data goes to 0x08020000, and:
__attribute__((__section__(".user_data"))) char userConfig[4] = {1, 2, 3, 4};
Is my user Data.
If I read it after flashing, I properly debug 1 2 3 4 values.
If I try to erase sector 5, it works and the values now display 255 255 255 255.
However, if I try to program anything, an HARD FAULT occurs (see code below).
Do you have any idea ?
FLASH_EraseInitTypeDef flashErase;
flashErase.TypeErase = TYPEERASE_SECTORS;
flashErase.VoltageRange = FLASH_VOLTAGE_RANGE_1;
flashErase.Sector = FLASH_SECTOR_5;
flashErase.NbSectors = 1;
uint32_t sectorError;
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR |
FLASH_FLAG_PGAERR | FLASH_FLAG_PGPERR |
FLASH_FLAG_PGSERR);
if (HAL_FLASHEx_Erase(&flashErase, §orError) != HAL_OK) {
error = true;
} else {
// If this is not used, the values correctly goes to 255, else an HARD FAULT occurs...
if (HAL_FLASH_Program(TYPEPROGRAM_BYTE, (uint32_t)&userConfig[0], 123) != HAL_OK) {
error = true;
}
}
HAL_FLASH_Lock();
- Labels:
-
DEBUG
-
Flash
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-09 3:53 AM
Pretty sure 123 isn't a valid address in this context​
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-09 3:56 AM
123 is not an address but a value, arguments of HAL_FLASH_Program are the type (BYTE, HALFWORD, WORD, DOUBLEWORD), the address and the data to be written
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-09 3:57 AM
Ultimately the code end up in FLASH_Program_Byte where the following is done:
*(__IO uint8_t*)Address = Data;
Address being 0x08020000 because it is the result of (uint32_t)&userConfig[0]
(I checked)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-09 6:04 AM
Duplicate:
What does the MCU say about the source of the hard fault?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-09 6:27 AM
Thanks @TDK​, I investigated the memory using STLINK debug and figured out that it was a MMARVALID + DACCVIOL fault, then I checked how the MPU is managed.
I am using MBED as environment and I missed this page that basically explains two of my problems.
The MPU is pre-configured by the framework to disable both writing in ROM and executing of RAM. You need to declare explicitly if you want it to be possible using `ScopedRomWriteLock` or `ScopedRamExecutionLock`
https://os.mbed.com/docs/mbed-os/v6.4/apis/mpu-management.html