cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446RE: can't call function in RAM

g239955_stm1
Associate II

If I try to put a method in the .data section using the below code, the microcontroller hangs when I try to call it. Is it a wrong way?

(When I check in the disassembly it appears indeed in the RAM)

__attribute__((long_call, section(".data"))) void my_ram_method() {
   // Do something
}

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Nikita91
Lead II

Perhaps an alignment problem...

__attribute__((aligned (4), section(".data"))) void my_ram_method()

Why the long_call attribute ?

g239955_stm1
Associate II

Actually, from the doc:

"

The CPU can access the SRAM1 and SRAM2 through the System Bus or through the I-

Code/D-Code buses when boot from SRAM is selected or when physical remap is selected

(Section 8.2.1: SYSCFG memory remap register (SYSCFG_MEMRMP) in the SYSCFG

controller). To get the max performance on SRAM execution, physical remap should be

selected (boot or software selection).

"

If I set SYSCFG_MEMRMP to 3 (to make SRAM1 appear to address 0) and then do the following, it is called successfully:

typedef void (*func)(void);
func prog = my_ram_method;
prog -= 0x02000000;
prog();

Still, it looks over-complicated

g239955_stm1
Associate II

About long_call, I thought it would help since the address of the RAM function is far with respects to the others, but I'm not sure it is necessary.

Uwe Bonnes
Chief

A least recent gcc does not need longcall

Uwe Bonnes
Chief

As long as the device has no RAM originally located below 0x20000000 (CCM Ram), expect collision between data and command access.

g239955_stm1
Associate II

Ok here is the actuel thing, I am using MBED as environment and I missed this page that basically explains two of my problems.

The MPU is pre-configured by the framework to disable both writing in ROM and executing of RAM. You need to declare explicitly if you want it to be possible using `ScopedRomWriteLock` or `ScopedRamExecutionLock`

https://os.mbed.com/docs/mbed-os/v6.4/apis/mpu-management.html