cancel
Showing results for 
Search instead for 
Did you mean: 

EMW3080 NetxDuo driver for STM32H5

AMend.7
Associate III

Hi, 

I would like to test the EMW3080 with the STM32H5, as I understand it is necessary to load the firmware provided by the ST in order for the EMW3080 to work with the driver provided for the B-U585I-IOT02A board. Correct?
Does ST have plans to launch any H5 kit with wifi, preferably using a wifi module with better support and availability, like the new nRF7002 and CC3301?

 

2 REPLIES 2
Foued_KH
ST Employee

Hello @AMend.7 , 

The MXCHIP EMW3080B firmware programmer is for the B-U585I-IOT02A board.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The WiFi firmware update for STM32H573I-DK + MB1400 daughter board with MXCHIP EMW3080B is also available at https://www.st.com/en/development-tools/x-wifi-emw3080b.html with the V1.1.0.
Some Wi-Fi examples for this board can be found under STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\Applications\NetXDuo\...
The Wi-Fi examples are the ones with the _wifi suffix.