cancel
Showing results for 
Search instead for 
Did you mean: 

DS12288 - STM32G474xB Datasheet - Errors

Singh.Harjit
Senior II
  1. Page 118, Table 38 has "1.78" in Peripheral column instead of TIM1.
  2. Page 115, fourth bullet says "... is given in Table 39. The power...". The table number should be 38.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee

Hello @Singh.Harjit​ ,

I think the first error is fixed in the DS12288 Rev 2.

Can you please check this ?

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Singh.Harjit
Senior II

Indeed it is! Thank you.

A couple minor items in Rev 2 - should I create a new thread since it is against Rev 2 and this thread has Rev 1 in the title?

  1. Section 2, page 13, half way down the page it says: twothree general-purpose 32-bit timers
  2. Section 3.6, page 19, Figure 2 shows SRAM1 on the I-bus and D-bus which doesn't match the description in section 3.5.

I was very glad to see the information in Tables 74 - 76.

Imen.D
ST Employee

Hello @Singh.Harjit​ ,

Thank you for pointing out the errors.

We will correct these in the next release of STM32G474 Datasheet.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen