2019-11-10 6:51 AM
Hi all,
I'm using nucleo STM32 L4R5ZI .
Using systick 120Mhz as clock
and set timer 2 , channel 1 as TIM_TS_TI1FP1 (Trigger and rising edge)
Then, using
int count = __HAL_TIM_GetCounter(&htim2); to sample the count for every 1ms.
Input 40KHz .
By right, the count for every 1ms is 40.
Somehow, a count will miss on every 4th ms, will be 39 for 4th, 8th 12thms.
Anyone has any idea what is going wrong?
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_SlaveConfigTypeDef sSlaveConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = TIMER_MAX;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;
sSlaveConfig.InputTrigger = TIM_TS_TI1FP1;
sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_RISING;
sSlaveConfig.TriggerFilter = 15;
if (HAL_TIM_SlaveConfigSynchro(&htim2, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */ int count = __HAL_TIM_GetCounter(&htim2);
2019-11-10 8:58 AM
One or both clocks (i.e. the external signal and the STM32 clock) may be unprecise. The difference is roughly 1 in 160, i.e. around 0.6%.
What is the primary clock source in STM32, MSI or HSI or HSE?
What is the 40kHz signal's source?
JW
PS. Please change your user name to a normal nick.
2019-11-10 9:35 AM
How good is your external clock source (HSE) or are you relying of VCO/PLL and HSI of some pretty arbitrary accuracy?
Perhaps quantify 120 MHz in TIM2 or TIM5 vs a GPS 1PPS input.
2019-11-11 2:08 AM
40k signal source is coming from function generator for testing.
I set to 120Mhz using PLL.
That is probably PLL clock is not accurate.
I should try from crystal oscillator
2019-11-11 2:09 AM
I'm relying on PLL.
Tim2 40Khz was coming from function generator.