2023-05-02 6:03 AM
Hello,
we currently have a problem using PB6 of an STM32G474ME as FDCAN-TX: During Reset, it is pulled down to GND, which we attribute to the USB-C functionality. This causes the FDCAN-TX line to send a dominant signal during reset of the STM32.
As per p. 72 of the datasheet for the STM32G474xE (DS12288 Rev 6) the pull-down should be disabled by pulling PA9 low. However, we cannot reproduce this, even though we can disable the pull-down of PB4 via pulling PA10 low.
Is our understanding of the issue correct? Can be pull-down-resistor of PB6 be disabled via other means?
Greetings,
Bernd
2023-05-02 8:12 AM
Hello @BGott.1 and welcome to ST Community :smiling_face_with_smiling_eyes:,
In order to disable the pull down on PB6, you only need to set UCPD1_DBDIS bit in the PWR_CR3 register.
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.