2022-07-10 12:29 AM
I am looking for maximum timer resolution supported in STM32U5 series MCU's.
Basically whether I can configure or use hardware timer as 100us.
Any input or documentation on this would be a great help.
Thanks!!
Solved! Go to Solution.
2022-07-10 5:55 PM
Interrupting at 1 MHz is not a sensible approach to any problem.
The TIM have resolution into the nano-seconds (6.25 ns).
I'd imagine there's a Reference Manual describing the hardware implementation, and a cook-book of related examples.
2022-07-10 1:21 AM
Every timer in every STM32 model may be setup according to your needs.
2022-07-10 5:55 PM
Interrupting at 1 MHz is not a sensible approach to any problem.
The TIM have resolution into the nano-seconds (6.25 ns).
I'd imagine there's a Reference Manual describing the hardware implementation, and a cook-book of related examples.
2022-07-11 12:24 AM
Thanks @gbm and @Community member for quick response.