cancel
Showing results for 
Search instead for 
Did you mean: 

does STM32H743 maximum gpios total current limit related to pin quantity? Datasheet says 140mA for 100,144,164.. pins.But i think max current must change base on pin quantity.

MZORE
Associate II

Are there anyone to know that gpio pin quantity to maximum current limit relation?

4 REPLIES 4
TDK
Guru

The datasheet certainly doesn't think so. Why would it change based on the number of pins?

If you feel a post has answered your question, please click "Accept as Solution".

Why, wouldn't it have more to do with the distribution of power, and the trace widths in the metal layers?

The parts share a common die, the bond out and lead frames might help localized current distribution/paths.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MZORE
Associate II

Because, more pin ,more vdd quantity i thought that more vdd more total gpio pin current out

MZORE
Associate II

for example at 100 pin 5 vdd, 144 pin 10 vdd existed , i thought that more vdd more bound out and more total gpio current