cancel
Showing results for 
Search instead for 
Did you mean: 

Does stm32f767zi support 3 CANs as slave?

ARam .1
Associate

in STMCubeMX it says that CAN1 and CAN3 are master and CAN2 is slave. I need to use all three CANs as slave.Would it be possible to do that? If i can do that would i just be configuring the CAN1 and CAN3 as master in STMCubeMX and continue to use them as slaves?

1 REPLY 1
Bouraoui Chemli
ST Employee

Hello @ARam .1​ 

Yes you can use CAN1 and CAN3 as master and continue to us them independently.

Best regards,

Bouraoui