2024-04-12 06:34 AM
Hi,
does have any line of STM32 possibility to measure 20 differential channels with voltages of about 100-150mV. So PGA will be welcome.
In classic parametric search, I cannot find such parameters.
Solved! Go to Solution.
2024-04-12 12:16 PM
Ah, sorry, I should have read your requirements more carefully. Correct, the PGA cannot process a differential signal.
I did a quick check and was able to assign 18 differential ADC channels to packages with 128 pins, you might be able to get 20 with a little rearranging. However, as the 150mV signals are somewhat small, in my opinion differential opamps or PGAs would have to be connected externally.
Regards
/Peter
2024-04-12 06:39 AM
Yes, just have a look at the family of STM32G4 providing up to 5 independent ADC with PGA.
Hope that helps?
Regards
/Peter
2024-04-12 07:35 AM
The G4 series cannot do it. They can use OPAMS as PGA but just with single ended signal (and have just a limited number of inputs to them). It has no way to convert differential signals to single ended ADC. And ADCs itself are just single ended without a gain stage.
2024-04-12 12:16 PM
Ah, sorry, I should have read your requirements more carefully. Correct, the PGA cannot process a differential signal.
I did a quick check and was able to assign 18 differential ADC channels to packages with 128 pins, you might be able to get 20 with a little rearranging. However, as the 150mV signals are somewhat small, in my opinion differential opamps or PGAs would have to be connected externally.
Regards
/Peter