Skip to main content
AE104
Associate III
April 9, 2024
Question

Parsing Raw Data

  • April 9, 2024
  • 12 replies
  • 5019 views

Hello,

I need to parse a raw data that I receive UART3 interface. Then, I will send to a PC to show results in serial monitor. Before implementing in the microcontroller, I tested my approach in a C compiler. A sample raw data in the buffer array and here is C code to do this job 

 

#include <stdio.h>
#include <string.h>
#include <stdlib.h>

int main() {
 char buffer[] = "e\nM0000\nPda7F85F3Fu;ba48D503Dp,10,288\nPda7F9234Bu;ba4E2C324p,10,288\nPda806EC24u;baAE16C6Dp,10,288\nPda807B031u;baB360495p,10,288\n*\n\n";
 char *token;
 token = strtok(buffer, "\n");
 int package_nr = 0;

 while (token != NULL) {
 if (strcmp(token, "e") == 0) {
 printf("Response begin\n");
 } else if (token[0] == 'M') {
 printf("Measuring...\n");
 package_nr = 0;
 } else if (token[0] == 'P') {
 if (package_nr++ == 0) {
 printf("Receiving measurement responses:");
 }
 printf("\n%d. ", package_nr);
 char *P = strchr(token, 'P');
 char *packageLine = P + 1;
 char *running = packageLine;
 char *param;
 while ((param = strtok_r(running, ";,", &running)) != NULL) {
 if (strlen(param) == 0) {
 continue;
 }
 char paramIdentifier[3];
 char paramValue[10];
 strncpy(paramIdentifier, param, 2);
 paramIdentifier[2] = '\0';
 strncpy(paramValue, param + 2, 9);
 paramValue[9] = '\0';
 printf("%s%s ", paramIdentifier, paramValue);
 }
 } else if (strcmp(token, "*") == 0) {
 printf("\nMeasurement completed.\n");
 printf("%d data point(s) received.\n", package_nr);
 } else {
 printf("%s", token);
 }
 token = strtok(NULL, "\n");
 }

 return 0;
}

 

Then I got this result:

 

Response begin
Measuring...
Receiving measurement responses:
1. da7F85F3Fu ba48D503Dp 10 288 
2. da7F9234Bu ba4E2C324p 10 288 
3. da806EC24u baAE16C6Dp 10 288 
4. da807B031u baB360495p 10 288 
Measurement completed.
4 data point(s) received.

 

 

 

To implement this code in the microcontroller, I simply removed the buffer array and replace it with Rx_Buffer which collects all raw data with HAL_UART_RxCpltCallback function. Then, here is the modified code:

 

 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 
	 char *token;
 char msg[100];
	 token = strtok(RX_Buffer, "\n");

	 while (token != NULL) {
	 if (strcmp(token, "e") == 0) {
	 sprintf(msg, "Response begin\n");
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 } else if (token[0] == 'M') {
	 sprintf(msg, "Measuring...\n");
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 package_nr = 0;
	 } else if (token[0] == 'P') {
	 if (package_nr++ == 0) {
	 sprintf(msg, "Receiving measurement responses:");
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 }
	 sprintf(msg, "\n%d. ", package_nr);
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 char *P = strchr(token, 'P');
	 char *packageLine = P + 1;
	 char *running = packageLine;
	 char *param;
	 while ((param = strtok_r(running, ";,", &running)) != NULL) {
	 if (strlen(param) == 0) {
	 continue;
	 }
	 char paramIdentifier[3];
	 char paramValue[10];
	 strncpy(paramIdentifier, param, 2);
	 paramIdentifier[2] = '\0';
	 strncpy(paramValue, param + 2, 9);
	 paramValue[9] = '\0';
	 sprintf(msg, "%s%s ", paramIdentifier, paramValue);
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 }
	 } else if (strcmp(token, "*") == 0) {
	 sprintf(msg, "\nMeasurement completed.\n");
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 sprintf(msg, "%d data point(s) received.\n", package_nr);
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 } else {
	 sprintf(msg, "%s", token);
	 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 }
	 token = strtok(NULL, "\n");
	 }
	 return 0;


	}

 

Then I got this result in the serial monitor:

 

Response begin
 e!0006Receiving measurement responses:
 1.

 


So what can be source of the problem?
Thank you,

 

This topic has been closed for replies.

12 replies

Pavel A.
April 9, 2024

Configure your terminal to handle \n as end of line (automatically add CR).

 

AE104
AE104Author
Associate III
April 9, 2024

Thank you @Pavel A. ! I set it CR, Both NL and CR but it didn't work. I also recgonized that after Rx_Counter reaches to 8, the code goes and stuck at Hardfault function.

 

Tesla DeLorean
Guru
April 9, 2024

Code snippet really doesn't convey broader context as to how you accumulate and hand-off the reception buffer.

The transmit calls here will block, consider creating an output ring buffer / FIFO

On the receive do this also with interrupts so you don't miss characters from you multi-character time blocking code.

Instrument HardFault_Handler() to output actionable data.

Likely faults due to exceeding buffers or pointers, or data buffers being out-of-scope.

Perhaps assumption buffers are NUL terminated when not, and using string functions.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AE104
AE104Author
Associate III
April 9, 2024

Thank you @Tesla DeLorean , here is the callback function to accumulate the raw data:

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{

 if (huart->Instance == USART3) // check if it's USART3 interrupt
 {
 RX_Buffer[RX_Counter++] = RX_Data[0]; // Store received data in buffer
 HAL_UART_Receive_IT(huart, RX_Data, 1); // Ready to receive next byte
 }

}

Can you give me an example for creating an output ring buffer / FIFO?

Tesla DeLorean
Guru
April 9, 2024

Providing source code is a bit beyond the scope of my participation here.

You should perhaps bounds check your RX_Counter, and look at how you determine a full/usable condition which you can flag, and move the content to a processing buffer, and restart your buffer acquisition here.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..