2017-01-30 10:38 AM
The reference manual, RM 00090, does not explicitly stay what happens to the GPIO lines when STOP mode is entered. If a pin is high, does it stay high?
#stop-mode #gpioSolved! Go to Solution.
2017-01-30 12:50 PM
RM0090, rev.13, p.122:
In Stop mode: the main regulator or low-power regulator supplies a low-power voltage to the 1.2V domain, thus preserving the content of registers and internal SRAM.
GPIO are no different from other peripherals.
JW
2017-01-30 12:50 PM
RM0090, rev.13, p.122:
In Stop mode: the main regulator or low-power regulator supplies a low-power voltage to the 1.2V domain, thus preserving the content of registers and internal SRAM.
GPIO are no different from other peripherals.
JW