2024-06-03 12:27 AM - edited 2024-06-03 12:36 AM
Hi everyone,
I'm facing an issue with using DMA1 for SPI communication in my project. I'm trying to achieve a 2 kHz frequency, but DMA1 doesn't seem to work at this rate, whereas BDMA functions without any problems.
This is my sampling task that is called with a timer interrupt,
if (!g_xGxStatus.txOngoing) {
g_xGxStatus.sampleReady = IsDataReady(&pxHandler->s1);
if (g_xGxStatus.sampleReady) {
g_xGxStatus.txOngoing = true;
HAL_GPIO_WritePin(pxHandler->s1.csPort, pxHandler->s1.csPin, GPIO_PIN_RESET);
HAL_SPI_TransmitReceive_DMA(pxHandler->s1.pxSpi, (uint8_t*) DMA_TxBuffer1, (uint8_t*) DMA_RxBufferGyro1, 6);
}
}
if (!g_xGyStatus.txOngoing && !g_xGzStatus.txOngoing) {
if (Sel == 2) {
g_xGyStatus.sampleReady = IsDataReady(&pxHandler->s3);
if (g_xGyStatus.sampleReady) {
g_xGyStatus.txOngoing = true;
HAL_GPIO_WritePin(pxHandler->s2.csPort, pxHandler->s2.csPin, GPIO_PIN_RESET);
HAL_SPI_TransmitReceive_DMA(pxHandler->s2.pxSpi, (uint8_t*) DMA_TxBuffer2, (uint8_t*) DMA_RxBufferGyro2, 6);
}
} else if (Sel == 3) {
g_xGzStatus.sampleReady = IsDataReady(&pxHandler->s3);
if (g_xGzStatus.sampleReady) {
g_xGzStatus.txOngoing = true;
HAL_GPIO_WritePin(pxHandler->s3.csPort, pxHandler->s3.csPin, GPIO_PIN_RESET);
HAL_SPI_TransmitReceive_DMA(pxHandler->s3.pxSpi, (uint8_t*) DMA_TxBuffer3, (uint8_t*) DMA_RxBufferGyro3, 6);
}
}
}
and also my the callback function for SPI Transmit-Receive:
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi) {
if (hspi->Instance == SPI2) {
HAL_GPIO_WritePin(g_xImuHandle.s1.csPort, g_xImuHandle.s1.csPin, GPIO_PIN_SET);
g_xGxStatus.sampleReady = false;
g_xGxStatus.txOngoing = false;
}
}
2024-06-03 1:02 AM - edited 2024-06-03 1:09 AM
Which 'H7?
> DMA1 doesn't seem to work at this rate
What are the symptoms?
Read out and check/post content of SPI and relevant DMA/DMAMUX registers, compare them to the working case, while figuring out differences using respective chapters in Reference Manual.
> BDMA functions without any problems.
I wonder, how could BDMA possibly work with SPI2, since there's no connectivity from SPI2 to DMAMUX2/BDMA.
JW
2024-06-03 1:14 AM - edited 2024-06-03 1:14 AM
Maybe it is the same issue I have?
Does your DMA maybe transfers no Data to the SPI peripheral?
2024-06-03 1:16 AM
Hi JW,
>Which 'H7?
It is STM32H735RGV.
>What are the symptoms?
I am getting either a 255 or 0 every 2-3 seconds. The data is also corrupted as well as the frequency.
>I wonder, how could BDMA possibly work with SPI2, since there's no connectivity from SPI2 to DMAMUX2/BDMA.
I am using BDMA via SPI6, I am simply configuring both SPIs and DMAs with the same configuration but I have connected 2 sensors to SPI6 so I use one of the sensors' CS in every cycle. Other than that the procedure is the same.
2024-06-03 1:19 AM
Hi,
I do not think so, as when I slow down my timer interrupt the DMA seems to be working fine.
2024-06-04 7:08 AM
I have realized that the data I have been sending through DMA was corrupted. I put the data to be sent at the address 0x30000000 for the SPI2 using DMA1 and for some reason the data I put in to the buffer changes at start up. I do not know how to place the buffer so that the data is not corrupted. I am also not using cache for that very same reason.7