cancel
Showing results for 
Search instead for 
Did you mean: 

DIY STM32F429 Evaluation Board

mc-4u
Associate
Posted on May 19, 2015 at 09:31

hello,

i would like to introduce my self-made Evaluation Board

for a STM32F429IGT6 (176 Pin LQFP)

pictures are attached

it's a 4 Layer 100mm x 50mm Board with onboard :

256MBit SDRAM

512kBit I2C-EEprom

16MBit SPI-Flash

CAN-Transceiver

FTDI-UART-Interface

Mini-USB for USB-OTG

Micro-SD-Card Connector

Six Status LEDs

And 2,54mm Header for many GPIOs and a 24bit TFT-Connector

(a second board for interfacing a 4,3 inch TFT is following)

here a link to my projectpage with further informations (only in german)

http://mikrocontroller.bplaced.net/wordpress/?page_id=4908

Uwe

#stm32f429
3 REPLIES 3
raptorhal2
Lead
Posted on May 19, 2015 at 16:02

Interesting. Even has 2 terminals for the ground clip of a VO meter or 'scope.

Does 1 row of the JTAG/SWD pins match the 4 pin SWIM in ST-Link V2 ?

Cheers, Hal

mc-4u
Associate
Posted on May 19, 2015 at 16:35

no, an adapter cable is needed

check theattached schematic

________________

Attachments :

f429_board_sch_v100.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0xH&d=%2Fa%2F0X0000000bki%2FP3Z0qsk17T1zjhT_urzNao9MY5rN3Z3dCObRgXjvStM&asPdf=false
qwer.asdf
Senior
Posted on May 19, 2015 at 17:23

@becker.uwe

Welcome to this forum Uwe, I hope you can hang with this community sometimes. Your blog is awesome, thank you for all the ub_* libraries that you've written for STM32F4, they helped me very much when I was starting STM32 microcontroller development.