2024-05-09 07:34 AM
Hello, as part of my master's, I am required to process information received from some electronic system, I need to read 36 bits (output of 3 12 bit ADC) at the same time and process them and perform calculations and for that I need execution speed. I chose STM32H743ZGT6 and I wanted to know if ports B,D,G,E in this microcontroller have direct access to SRAM memory for fast reading of the ports and the possibility to process them after 4 clock cycles? That is, they will be stored in SRAM after 4 clock cycles
2024-05-09 07:35 AM
And if not , if there is any another option to do that?
2024-05-09 07:50 AM
2024-05-09 11:43 AM - edited 2024-05-09 11:55 AM
Hi,
for really fast port access - the H7 is not the best choice. (very complex architecture, ports "far away" from core/ram)
Ports are on AHB4 bus and so on its speed there...see ds .
>possibility to process them after 4 clock cycles
Well, maybe ... fastest i got : 25ns at 200M core , so 5 core clks.
You will use DMA for this - right ? So just try (I didnt.), how many clks to RAM.
Maybe using BDMA -> to local 64KB RAM, it could be very fast (1 AHB4 clk , 4ns ?) and it dont block core, working on other RAM ....try it! and tell... 🙂
Compare with a H563 , i got : 4ns at 250M core, so 1 core clk.
Here ports on AHB2 bus with direct access from core :
So a "more simple" architecture much better for a "simple" port access from core.
2024-05-09 01:27 PM
Congrats, your description is vague and unclear to the point of nonsensical.
"4 clock cycles": there's only about 137 clocks in the H7. Do I get to pick?
"possibility to process": details matter.
People here will go out of their way to help and try to winkle out enough information to do so properly but questions like this really deserve only a resounding "Maybe, it depends.". Try again, with some actual explanation.