2021-04-25 10:53 PM
2021-04-26 01:47 AM
Hello,
Welcome to STM32 Community!
Please refer to section 2 of Application note AN4195 available on our website.
I recommend you to have a look to Reference Manual which included the necessary details.
Imen
2021-04-26 06:36 AM
if i remember correctly...
Regular mode: the adc converts one or multiple times by its own.
Injected mode: the adc conversion is triggered by an event like a timer or interruption or software.
I dont like the naming of these modes, its confusing.
2021-04-27 02:48 AM
Thanks for your reply Mr.Imen GH. Im new to STM and im using stm32f469i-Discoivery board,But the manual you suggested to me is for only f1 and f3 series..
My question is there any individual documentation for specific modules(i.e ADC,timer and so on.) or the reference manual is the only key?
2021-04-27 02:49 AM
Thanks javier for your valuable concern.
2021-04-27 03:24 AM
Hello,
The concept is also valid for STM32F4 product.
The reference manual contains essential information and full details.
Imen