2023-03-02 1:34 AM
When I use DFSDM, I configure FOSR= 256 ISOR=1 and the output is outside the range in the reference guide +-16777216
Solved! Go to Solution.
2023-03-02 4:35 AM
Get the answer
/* Regular conversion value is a signed value located on 24 MSB of register */
/* So after applying a mask on these bits we have to perform a division by 256 (2 raised to the power of 8) */
2023-03-02 1:56 AM
Hello @GWenJ.1 and welcome to the Community :)
Please specify which device used?
You can check the STM32Cube package which providing DFSDM example that can help you on the DFSDM usage and configuration.
Imen
2023-03-02 2:33 AM
STM32H723
The STM32Cube H7 package which providing DFSDM example,Only refer a applicableation About Audio
Can you verify the range of DFSDM output results at FORD=3 FOSR=256 ISOR=1 ?
2023-03-02 3:28 AM
A
2023-03-02 4:35 AM
Get the answer
/* Regular conversion value is a signed value located on 24 MSB of register */
/* So after applying a mask on these bits we have to perform a division by 256 (2 raised to the power of 8) */