cancel
Showing results for 
Search instead for 
Did you mean: 

Demonstration source code for AN3126

sirdancesalot
Associate

I have been looking into Application Note AN3126 (Audio and waveform generation using the DAC in STM32 products) and in the document a demonstration source code project is mentioned which includes C-language files waveplayer.c and waveplayer.h. I was unable to find this mentioned demo project. Can you help me locate it? Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @sirdancesalot and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to take a look at this post. It will answer your question.

PS: this demonstration is build for The STM32100B-EVAL wish is an obsolete board. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @sirdancesalot and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to take a look at this post. It will answer your question.

PS: this demonstration is build for The STM32100B-EVAL wish is an obsolete board. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

hayat
Associate III

 

Hopefully, the attached document can be used and adapted for your platform.