cancel
Showing results for 
Search instead for 
Did you mean: 

Delay, multi milliseconds, on the STM32F0, again..

XooM
Senior

where I wrote it among the codes.. // Here I have to wait 500ms.
Can you help me to prevent the timers from being affected by this wait?
Can you give me the codes that I will add. Because I am very confused..

I tried many things but they all stopped the interrupts..

 

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { if(htim->Instance==TIM1) { if(input1==0) { HAL_GPIO_WritePin(GPIOA, GPIO_Pin_1, GPIO_PIN_SET); // Here I have to wait 500ms. HAL_GPIO_WritePin(GPIOA, GPIO_Pin_1, GPIO_PIN_RESET); } }

 

 

 

 

 

70 REPLIES 70

I don't understand what you mean, but I'm sure I can understand it more easily if you explain it only through my code. Could you please intervene in my code?

No, it does not reset. PinA10 always remains in the SET position.

This is perfectly normal when input1 == 1 time is ? You ignore reply to questions 

 

All inputs are pull-up when they are idle..
If the input comes, they become "0"..

I ask time , you reply other... FYI Input1 10ms 0 and 500ms 1 after this 10ms 0

Result is your PA10 always SET. Or for detail is RESET for 10ms and set back.

But optimal is debug your code with breakpoints and check if code parts is realy executed.

volatile uint8_t input1 =1,input2 =1;

updated in ISR require volatile...

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ volatile uint32_t Tick_PA2_On; // Time it was turned ON volatile int PA2_On = 0; // Flag that is is ON uint8_t input1 =1; uint8_t input2 =1; uint8_t m =0; uint16_t currentVal=0; uint16_t led1=0; /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ TIM_HandleTypeDef htim1; TIM_HandleTypeDef htim2; TIM_HandleTypeDef htim16; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_TIM1_Init(void); static void MX_TIM2_Init(void); static void MX_TIM16_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ #define SER_PIN GPIO_PIN_4 // SER_PIN #define SER_PORT GPIOB #define SRCLK_PIN GPIO_PIN_12 // SRCLK_PIN #define SRCLK_PORT GPIOA #define RCLK_PIN GPIO_PIN_5 // RCLK_PIN #define RCLK_PORT GPIOB void HC4094write() { HAL_GPIO_WritePin(RCLK_PORT, RCLK_PIN, GPIO_PIN_RESET); for(int i=0; i<16; i++) { if(currentVal & (1<<i)) { HAL_GPIO_WritePin(SER_PORT, SER_PIN, GPIO_PIN_SET); } else { HAL_GPIO_WritePin(SER_PORT, SER_PIN, GPIO_PIN_RESET); } HAL_GPIO_WritePin(SRCLK_PORT, SRCLK_PIN, GPIO_PIN_RESET); HAL_GPIO_WritePin(SRCLK_PORT, SRCLK_PIN, GPIO_PIN_SET); } //HAL_GPIO_WritePin(RCLK_PORT, RCLK_PIN, GPIO_PIN_RESET); HAL_GPIO_WritePin(RCLK_PORT, RCLK_PIN, GPIO_PIN_SET); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_TIM1_Init(); MX_TIM2_Init(); MX_TIM16_Init(); /* USER CODE BEGIN 2 */ HAL_TIM_Base_Start_IT(&htim1); HAL_TIM_Base_Start_IT(&htim2); HAL_TIM_Base_Start_IT(&htim16); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { if (PA2_On) { if ((HAL_GetTick() - Tick_PA2_On) >= 500) // On for 500ms, turn it off now { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_RESET); PA2_On = 0; } } /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief TIM1 Initialization Function * @PAram None * @retval None */ static void MX_TIM1_Init(void) { /* USER CODE BEGIN TIM1_Init 0 */ /* USER CODE END TIM1_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM1_Init 1 */ /* USER CODE END TIM1_Init 1 */ htim1.Instance = TIM1; htim1.Init.Prescaler = 1199; htim1.Init.CounterMode = TIM_COUNTERMODE_UP; htim1.Init.Period = 5; htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim1.Init.RepetitionCounter = 0; htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE; if (HAL_TIM_Base_Init(&htim1) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM1_Init 2 */ /* USER CODE END TIM1_Init 2 */ } /** * @brief TIM2 Initialization Function * @PAram None * @retval None */ static void MX_TIM2_Init(void) { /* USER CODE BEGIN TIM2_Init 0 */ /* USER CODE END TIM2_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM2_Init 1 */ /* USER CODE END TIM2_Init 1 */ htim2.Instance = TIM2; htim2.Init.Prescaler = 11999; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; htim2.Init.Period = 1; htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE; if (HAL_TIM_Base_Init(&htim2) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM2_Init 2 */ /* USER CODE END TIM2_Init 2 */ } /** * @brief TIM16 Initialization Function * @PAram None * @retval None */ static void MX_TIM16_Init(void) { /* USER CODE BEGIN TIM16_Init 0 */ /* USER CODE END TIM16_Init 0 */ /* USER CODE BEGIN TIM16_Init 1 */ /* USER CODE END TIM16_Init 1 */ htim16.Instance = TIM16; htim16.Init.Prescaler = 11999; htim16.Init.CounterMode = TIM_COUNTERMODE_UP; htim16.Init.Period = 1; htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim16.Init.RepetitionCounter = 0; htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE; if (HAL_TIM_Base_Init(&htim16) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM16_Init 2 */ /* USER CODE END TIM16_Init 2 */ } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, Q1_Pin|Q2_Pin|Q3_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(Q5_GPIO_Port, Q5_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : input2_Pin */ GPIO_InitStruct.Pin = input2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(input2_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : input1_Pin */ GPIO_InitStruct.Pin = input1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(input1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : Q1_Pin Q2_Pin Q3_Pin */ GPIO_InitStruct.Pin = Q1_Pin|Q2_Pin|Q3_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pin : Q5_Pin */ GPIO_InitStruct.Pin = Q5_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(Q5_GPIO_Port, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { //I turn on/off 24 LEDs according to the inputs. if(htim->Instance==TIM1) // Timer2 Update Event'i 250us { } //I manage the outputs according to the incoming inputs. if(htim->Instance==TIM16) // Timer16 Update Event'i 1 ms { if(input2==0) { if(input1==0 && PA2_On ==0 ) { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_SET); Tick_PA2_On = HAL_GetTick(); PA2_On = 1; } else { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_SET); } } else { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET); } } // I use it to assign inputs and outputs to variables. if(htim->Instance==TIM2) // Timer2 Update Event'i 1 ms { input1 =HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_2); input2 =HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13); } } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

The code above is the code, there is no other code..

Remove TIM2 from your code is waste of timer with same base time. And change code 

 

/* USER CODE BEGIN 4 */ void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { //I turn on/off 24 LEDs according to the inputs. if(htim->Instance==TIM1) // Timer2 Update Event'i 250us { } //I manage the outputs according to the incoming inputs. if(htim->Instance==TIM16) // Timer16 Update Event'i 1 ms { if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)==0) { if(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_2)==0 && PA2_On ==0 ) { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_SET); Tick_PA2_On = HAL_GetTick(); PA2_On = 1; } else { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_SET); } } else { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET); } } } /* USER CODE END 4 */
View more

 

When Pin_A2 is "0", Pin A10 becomes "1".
Continuing..
If Pin_A2 becomes "1", Pin A10 becomes "0" after 500ms.
That is, it works in reverse.
There is no delay when the input comes
It waits for 500ms when the input disappears.

 

Note1 : I am writing with Translate, I hope I can explain.

Note2:

The program is currently running as follows.

When C13=1 and A2=1, A10=0
When C13=0 and A2 =0, A10 =1
500ms after C13=0 and A2 =1, A10 =0
It drops to 0 not when the input arrives, but after the input disappears.


@XooM wrote:

When Pin_A2 is "0", Pin A10 becomes "1".
Continuing..
If Pin_A2 becomes "1", Pin A10 becomes "0" after 500ms.
That is, it works in reverse.
There is no delay when the input comes
It waits for 500ms when the input disappears.

 

Note1 : I am writing with Translate, I hope I can explain.

Note2:

The program is currently running as follows.

When C13=1 and A2=1, A10=0
When C13=0 and A2 =0, A10 =1
500ms after C13=0 and A2 =1, A10 =0
It drops to 0 not when the input arrives, but after the input disappears.


You need a truth table. So far from the code you've posted and your last post, I've made this table. There are some unknowns of what PA10 state is, so I left those blank.

You need to fill in the blanks so we really know what you're trying to accomplish with all the outputs based on all the input states.

KarlYamashita_0-1731532980287.png

 

If you FIFO doesn't work, then it's called GIGO.
TimerCallback tutorial! | UART and DMA Idle with multiple UART instances tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

 

 

Mi