Debugging probe StLink V3. GND Detect input (?) signal. What is the minimal set of connections essential? What about VCC input?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-05-31 11:20 AM
Hello,
I connected my probe StLink V3 MODS via only: GND, SwClk, SwDio (CN2.pin8.13,4) for the beginning. And it rather works. Rather as once I got a strange message instead of debugging.
I would like to have my probe reliable so I have found that I have the "GND Detect" signal unconnected (CN2.pin5, CN5.pin11). The datasheet says: "Connect to GND on target, may be used by STLINK-V3MODS for detection of connection." But what does this "... may be used..." really mean: . Should I connect? Or must? Or must not?
What if I do not connect?
To check, I have pulled it up (CN2.pin5) to 3v3 via 5K6 and... found 14 mV on this pin. But it is claimed as "input". Such a heavy input?
Finally, I have shorted CN2.pin5 to GND (CN2.pin8) (as I have no extra GND pin on target connector). Is it correct? Is it necessary?
And by the way. What is the T_VCC input (CN2,pin30, CN5.pin3 ) for?
Regards
Robert
- Labels:
-
DEBUG
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-05-31 12:09 PM
Means it loops back, both pins are ground at the target boards header, so it can see the cable is present and plugged in, end-to-end
T_VCC the Target's supply, so the ST-LINK can measure and report this voltage in STM32 Cube Programmer, etc. In other designs it would allow the JTAG pod side buffers/translators to be powered.
For "Connect Under Reset" to work the NRST pin needs connectivity. For SWV operation the SWO (PB3) needs connectivity.
Up vote any posts that you find helpful, it shows what's working..