2023-07-30 08:58 AM
I am trying to debug my Nucleo H723ZG board using the CN5 (MIPI10) and a Segger J-Link Pro. But I have tried both methods described in the UM2407 6.3.3 "Using an external debug tool to program and debug the on-boards
STM32H7" and neither allows the J-Link to connect to H7. When I attempt to start a debugging session, I get the following error message:
And the J-Link startup dialog looks like this:
SEGGER J-Link GDB Server V7.84e Command Line Version
JLinkARM.dll V7.84e (DLL compiled Feb 1 2023 16:41:41)
Command line: -port 2331 -s -device STM32H723ZG -endian little -speed 4000 -if swd -vd
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: off
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: STM32H723ZG
Target device parameters: none
Target interface: SWD
Target interface speed: 4000kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Link Pro V4 compiled Sep 22 2022 15:00:37
Hardware: V4.00
S/N: 174403180
Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
Checking target voltage...
Target voltage: 3.32 V
ERROR: Failed to listen at socket (Err = -1)
ERROR: Failed to open listener port 2331
Restoring target state and closing J-Link connection...
Shutting down...
Failed to open listener port 2331
This appears to be an issue with the GDB server, but I can't figure out why? Or perhaps it might be that the CPU is not running?
Any thoughts would be appreciated.
Thanks,
MikeH
2023-07-30 10:01 AM - edited 2023-07-30 10:48 AM
the CN5 connects to the onboard st-linkV3 . did you disable this ?
so dont connect j-link , use the onboard st-linkV3 , connect PC to CN1 USB (micro usb probably).
is it (still) working?
2023-07-31 06:53 AM
AScha,
"so dont connect j-link , use the onboard st-linkV3 ,"
I need to use the J-link for more complex dual-board debugging. I don't want to use the on-board ST-Link.
"the CN5 connects to the onboard st-linkV3"
..not according to the documentation. CN5 is the MIPI debugging connector as shown below.
"did you disable this ? "
I did jumper the STLINK-RST pin, but this appears to also disable the power supplied to the CPU. My J-Link cannot connect to the CPU.
Again, I prefer to use the more powerful J-Link Pro for debugging. How can I do this with the Nucleo board?
Thx,
Mike
2023-07-31 07:19 AM - edited 2023-07-31 07:23 AM
ok, so you want/need j-link...hmm.
look at circuit:
https://www.st.com/en/evaluation-tools/nucleo-h723zg.html#cad-resources
jumper the STLINK-RST pin, ok. but seems, hse + lse not fitted on board, so you cannot run with external clocks, except you have mount them on board + connect (solder bridges); (and st-link under reset -> no clock to H7 cpu !)
then decide, how to power it...and st-link needs to be powered also, even in reset, because connects also to cn5.
you should get connect with j-link, "under reset", because cpu starting then on internal HSI clock.
so: some work, to run it with j-link. 🙂
2023-07-31 07:53 AM
Probably move jumper from JP3 to JP1. And JP2 to CHGR if using USB-C to power.
2023-07-31 11:40 AM
Tesla, "Probably move jumper from JP3 to JP1. And JP2 to CHGR if using USB-C to power"
This does let the J-Link to connect to the MCU, but as mentioned by Ascha, the chip is now not receiving a clock from the debugger. Seems a bit confusion that the documentation clearly implies that this can be done.
6.3.3 Using an external debug tool to program and debug the on-boards
STM32H7
There are two basic ways to support an external debug tool:
1.Keep the embedded STLINK-V3E running.
Power on the STLINK-V3E at first until the COM LED lights RED. Then connect your external debug tool through the MIPI-10 debug connector (CN5).
2. Set the embedded STLINK-V3E in the high-impedance state:
When the STLK_RST jumper (JP1) is ON, the embedded STLINK-V3E is in the RESET state, and all GPIOs are in high impedance. Then it is possible to connect the external debug tool to the debug connector (CN5).