Debugging crashes at the middle of the program
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 1:35 AM
Hi All.
I am using:
IDE: System Workbench
Board: Nucleo L476RG
MCU: STM32F031G6U6
At first debugging starts without any issues. But then at some point in the program I get the error
No source available for '0x1fffedba'
I made a demo video to explain the problem better.:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 3:17 AM
is the chip getting hot ?
can you hold your finger on ?
Start from cold, see how long it takes to get hot.
on my desk the F091 is reporting an internal temp of 37.7C, slightly warm to touch.
do you have cache turned on ?
is it a custom board ?
you could check the voltage on Vdda/Vdd/Vss pins, see if it is stable and fairly noiseless.
is Boot0 floating ? and NRST ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 4:30 AM
Stack overflows or gets trashed and jumps into ROM?
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 7:50 AM
Thank you guys for reponding.
I troubleshooted the problem and discovered that when I comment one line, the MCU works just fine.
This is the code:
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
/*SysTick_CTRL_TICKINT_Msk |*/ SysTick_CTRL_ENABLE_Msk; /* Enable SysTick IRQ and SysTick Timer */If I remove the comment from the line in bold, the micro hangs again just as in the video.
The original code is like this:
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
SysTick_CTRL_TICKINT_Msk | SysTick_CTRL_ENABLE_Msk; /* Enable SysTick IRQ and SysTick Timer */The
SysTick_CTRL_TICKINT_Msk
is Bit-1
SysTick Control and Status register.
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0662b/Babieigh.html
.I suppose that there is a missing function that handles the interrupt request.
So I defined SysTick_Handler and now the code look like this:
#include 'stm32f031x6.h'
#include 'main.h'#include 'stm32f0xx_hal.h'void SystemClock_Config(void);
static void MX_GPIO_Init(void);volatile uint32_t vect = 0;
void SysTick_Handler(void)
{ HAL_IncTick(); vect++;}int main(void) {
HAL_Init();
MX_GPIO_Init();HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
while(1) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);}
/* Configure the system clock */}static void MX_GPIO_Init(void){GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);/*Configure GPIO pins : PA4 PA8 */
GPIO_InitStruct.Pin = GPIO_PIN_8 | GPIO_PIN_4; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);}
But still the same error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 8:11 AM
Please see the comment above I edited it. It is basically impossible to have a stack overflow. It may not be linked, but how would I know?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 9:55 AM
Suggests you're missing the handler, or linkage to the one in the vector table.
void SysTick_Handler(void)
{}
Or calling it causes the stack depth to be exceeded due to stacking context, or call tree below the handler and callbacks.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 10:16 AM
the code you commented starts the systick. I would check to see
1) if systick is initialized somewhere else;
2) if the systick interrupt is already somewhere else;
3) what HAL_IncTick() does;
4) if systick is firing and if the ISR gets executed;
...
basically trimmed your code to a basic set and go from there.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-21 10:21 AM
You could probably look at the .MAP or .LST listing file, or generate a disassembly?
Going to be expecting the Vector Table to be at 0x08000000, and one of the entries is going to be pointing to the handler.
Dump the 32-bit words at 0x08000000, and SysTick should be at 0x0800003C as I recall.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-22 3:16 AM
Looking at the Reference Manual I see that the vector table for this chip starts from 0x00000000.
Then I checked the values of these addresses and saw nothing like 0x0800 ....
This is the debuggers view of these addresses:
It seems to me that the the vector table is nit initialized at all.